Pulse Edge Time

The edge times set the transition times for the leading and trailing edges of the pulse. The edge time represents the time between the 10% and 90% thresholds.

Note: The specified edge time must fit within the specified pulse width. The function generator will adjust the edge time as needed to accommodate the specified pulse width.

See Also

Pulse Period

Pulse Width